according to the spec, if the EN pin is pulled lower than 1.2V
the switcher is turned off
i have turn off my tps54540 dda part with the EN pin below 0.6v
but i still see at least 1.5v at the switcher output
why is that so?
i need to turn off the switcher completely
there are no other voltage on the pcb other than the incoming 12VDC and it is only going into the tps54540 input and to the EN pin via a 100k resistor
my email: johntse@asis-technologies.com
john