Other Parts Discussed in Thread: BQ34Z100EVM, EV2400, GPCCHEM, BQSTUDIO, , BQ34Z100
Hello,
First here my settings:
- BQ34Z100EVM
- EV2400, version 18
- Lead Acid battery, 12V 7Ah
- BQ Studio, version 1.3.86
I have already done these things:
- Current and voltage calibration
- Find the Chemical ID using the GPCCHEM tool
But now I have two problems to end the calibration:
- I want to change the value of “Design Capacity”, “Terminate voltage” and other things but bqStudio tells me “a read of data written failed comparison”. It don’t change the value. I have tried many things: UNSEAL FULL ACCESS, ENTER_CAL, CAL_ENABLE. I have also tried to use the BQ studio version 1.3.54.1 but I get the same message. I can I fix this?
- How should I do the learning cycle? Is only one cycle enough? I there a special way to discharge the battery? Do I have to send specific commands to the BQ34Z100-G1 or will it do the calibration automatically?
Thank you in advance and sorry for my bad English,
Guénolé