This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] TPS2373-4EVM-758: Active Bridge Rectifier Disconnect Circuit (Q18)

Prodigy 380 points

Replies: 1

Views: 277

Part Number: TPS23754

Hi Sir,

There is an Active bridge design on the TPS2373-4EVM-758 and we applied it with TPS23754 design. 

1. May I know what's the purpose of the Q18 on the active bridge circuit? Do we still need to add Q18 circuit if we design a divider resistor to pull high the APD pin?   

2. If we design a divider resistor to pull high the APD pin, the active bridge could be totally shut off? 

  • Hi Teresa,

    Q18 is needed to turn off the active bridge circuit to prevent additional current leakage from Vdd to Vss to minimize power consumption when Auto MPS is used to keep the PSE port awake while the adapter is providing power.

    Thanks,
    Tom Amlee
    PoE PD Apps Engineer

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.