Other Parts Discussed in Thread: BQ2432,
I have implemented the reference Design of the BQ2432 in a commercial application.
We are now facing issues with returns due to the charger not charging the battery anymore
I have set the charging current to 200mA which I can verify with a DMM,
I have set the Iterm to about 10mA which works
The battery is a 250mA capacity.
The Input is from a usb, through a ferrite bead and a capacitor of 10uF /16V . The output capacitor is as rated 4.7uF/16V. TS is disabled (set to 10kOhm)
ILIM 2.94k, ISET 4.32k .
The problems we have faced with about 10 or so boards out of the 400
1) With only battery connected, IN is outputing voltage ; about 3.5V and has a sourcing current of about 2.7mA
2) Even though a charger is connected and outputing voltage, PGOOD goes low, CHG does not begin even with a good battery (VBAT>3.7V) The current draw from the charger is about 20mA constant.
3) Battery drops to Zero. I though that it disconnects the OUT from BAT when voltage drops below a certain value to protect overdischarge
Thank you in advance