• TI Thinks Resolved

TPS63036: Input Voltage Range

Prodigy 70 points

Replies: 2

Views: 60

Part Number: TPS63036

Hello,

I want to use TPS63036 Buck Boost Convertor for converting 3-6 V Input range to 5 V output. I am using two 3 V coin cells in series as Vtg source.

Is it OK if 6 V input is given as input to the convertor, its range is given as 1.8 V to 5.5 V, but absolute maximum input voltage is 7 V.

Will this configuration be stable.

If not please suggest similar part.

Thanks,

Ameya