Other Parts Discussed in Thread: BQ40Z50
Hello,
I am interested in making use of the fast charge function built into the Advanced Charge Algorithm available with the bq40z50. My understanding is that because I have set the SOC_CHARGE bit in Charging Configuration register, RelativeStateOfCharge() will be used instead of the voltages threshold control for the Low, Medium and High charge rates - is this correct? I am planning to use the default SoC Range thresholds of;
SoC Med: 50%
SoC High: 75%
Hysteresis: 1%
Assuming the battery temperature remains in the Recommended Temp (RT) range (between T5 and T6), does this mean that the charge current will be set as follows;
RelativeStateOfCharge(0-50%): RT CCH
RelativeStateOfCharge(50-75%): RT CCM
RelativeStateOfCharge(75-100%): RT CCL
Thank you,
Jeremy.