Other Parts Discussed in Thread: LM73605, LM43601, TPS54541
Hi Ti family.
In my design there will 4 different voltage levels.
Voltage input: 11V to 24V but for safety max will be more than 30V. ( transients)
Outputs:
1.2V 8A / 3.3V 4A / 2.5V 1A / 10V 5A
I plan to use TPS40170.
** In my system there is no air flow.
Is it a good choice?
Thanks