Other Parts Discussed in Thread: LMG1020, UCC27611, CSD17381F4, LMG1205, LMG1210
Dear All,
i need to pulsed an uv-led with a frequency from 100kHz ( 5 us on, 5 us off) to 1 MHz ( 500ns on 500ns off) with few ns of rise/fall time. I'm thinking to use a fast mos driver like the lm5112 (or if you know something better) plus a fast switching mosfet. The led had a working point between the 6-7V and the current will be between 5 and 30 mA.
Did you have any suggestion about the mosfet to use and if there is something betther than the lm5112 for my purpose? (Maybe the lmg1020, but i never used GaN mos).
Actually i'm simulating my circuit with Tina.
Thanks in advance.