This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] BQ24610 & BQ24650: BQ24610 & BQ24650 Schematic Review Design Tips

Expert 8305 points

Replies: 1

Views: 3118

Part Number: BQ24610

What are some key considerations when designing a schematic using BQ24610 or BQ24650, and what can I do if I want to simplify external component count by disabling some features?

Regards,

Kedar Manishankar

Applications Engineer

Please click "This resolved my issue" button if this post answers your question

  • The following document shows key considerations when choosing external components for your BQ24610 or BQ24650 design, as well as the tradeoffs. BQ24610 is a standalone 1-6 cell customizable charge controller, and the document also shows a simplified schematic if customer does not want to use PowerPath or DPM feature. This document also details external component selection for BQ24650 - a standalone 1-6 cell charge controller with integrated Maximum Power Point  Tracking. Using this information, customer can reduce external components based on their application, as well as use this document to help in assisting with schematic reviews.

    Note that the BQ24610 schematic description shown below is also applicable when designing systems with BQ24617.

    BQ24610_BQ24650_Schematic_Checklist.pdf

    Regards,

    Kedar Manishankar

    Applications Engineer

    Please click "This resolved my issue" button if this post answers your question

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.