Other Parts Discussed in Thread: BQSTUDIO
I'm using BQ27GDK000EVM with BQ27530EVM everything seems to work. I can charge and discharge my battery.
1. Although I'm unable to get device to charge battery to any other voltage than 4.2V, that appears to be default value. I can read and write from data memory, but it seems that these numbers do not take action. Are these (see picture below) the only three requirements for charging termination? Or is it related with Chemistry chosen?
2. What impact on charging does chosen Chemistry has? I don't see it changing any other memory parameters than "Chem ID".
3. Can I control Charging type (CC/CV) ? Now it is charging with CV.
Attached my register values: