hi,
we are considering the bq24773 for a 2S Li-Ion charger.
As far as I understood, at power up default settings are (CELL is left floating for a 2S config.):
ChargeVoltage() = 8400mV
ChargeCurrent() = 2944mA
MaxChargeVoltage() = 9008mV
MinChargeVoltage() = 6144mV
What I didn't understand is what is the SYS level after soft-start is over.
8.4V?
Vbat + little Drop-out?
thansk a lot in advance
KR
Vincenzo