Dear all,
I encounter an issue with some of my devices that includes 4 BQ24103A in parallel.
These devices are sold in Mongolia and there storage conditions are very hard: my devices have been stocked by -40°C.
I sold 10 devices and among them 4 have encountered the problem: the 4 BQ of each device were out of order (either there was no detection signal on output pins or there were no modification on STAT1 pin by connecting the battery).
Do you think there is a link between staorage conditions and high ratio of failure even if the chip is given to be stocked down to -65°C?
Thanks for your help.
Kind regards,
Nicolas.