Other Parts Discussed in Thread: LM5050-1,
Team,
we were testing LM74700 as ideal diode for reverse input protection (max input voltage is 60Vdc). We follow schematic from figure 19 on page 15 of the datasheet.
The device works well when tested for positive surge impulse, but it is getting destroyed on negative surge impulse (standard surge test according to EN 61000-4-5. Voltage 1kV, 2kV impulse. Coupling between plus and minus, generator has impedance 2 Ohm, coupling through capacitor 18uF.)
On input we have overvoltage protection, varistor and transil (SM15T68CA).
Tried also LM5050-1, result is the same (here used schematic from page 20, figure 31 on the datasheet).
What can be the issue?
Thanks for your help,
TI Customer