Other Parts Discussed in Thread: BQSTUDIO, EV2400
Hi all,
I am using bqStudio software.
Can I generate the *.gg.csv configuration file offline (without connecting EV2300 or EV2400 to the PC).
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Az,
If you want to Export Defaults (only option if you do not have hardware connected), you need to go to Windows->Preferences and click on 'Show Advanced Views', then click 'Apply'. This will enable the feature to Export Defaults.
Best regards,
Matt
Thanks Matt for your helpful reply.
I can now generate the .gg.csv file (offline) containing the default flash data values.
I have a battery pack with 2-cell in series (each one 3.7 V) and with a capacity of 3000 mAh.
Can I generate the .gg.csv file corresponding to this battery pack offline ?
Hi Az,
This doesn't really work without hardware connected. You can edit the .gg.csv directly outside of BQStudio (use a text editor because saving in Excel can cause issues), but you really will not be able to verify the settings are working correctly without hardware connected.
regards,
Matt