Hello
On page 3 of the DCP020507 datasheet in the device comparison table, it says that the output voltage @75% load will be within 5% of the nominal output voltage: 6.65-7.35V
This for an input voltage of 5V ± 10%.
1) How can the tolerance of the output voltage be smaller than the input voltage if the device is unregulated?
2) I made a few quick tests with DCP020507 and the relative output voltage error had more or less a 1:1 ratio with the input voltage error
How can this be explained? What am I missing?
Best regards
Haje