Hi,
I'm evaluating LM5160 on LM5160DNTFBKEVM(Flybuck topology) and set external components based on calculator as attached.
LM5160FBKQuickStartCalculator - FinalVersion 20190625.xls
VIN=24V, Vout-pri=12V, ; Iout-pri=0A, Vout-sec=11.4V, Iout-sec=1.1A
Coupled Inductor: 744873680
This circuit is not working correctly, and secondary output voltage is 3V which is lower than setting voltage(11.4V).
This voltage drop depends on Iout-sec.
What is this voltage drop caused by?
I guess that the delay from SW-pri on to SW-sec off occurs because the delay also depends on Iout-sec.
Best Regards,
Kuramochi