hi team,
Set the input voltage change from 41v to 55V(the time is 10ms)
Set the output current to 5A
Delay 1s
Set sample number to 2048( time will be 2s)
Delay 2s
When we test the 55V, sometimes the input isn't accurate (53v sometimes).
So we want to check the reason, whether the when set the sample number, whether the device start to sample the 2048 times during that time? So the register hasn't been updated, Thanks.