This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62060: datasheet Question

Part Number: TPS62060

Hi everybody!

I have a question about the "TPS62060" datasheet.

Q1)
The absolute maximum rating of the SW terminal is described as -0.3 V to 7 V in the datasheet of this device.
In the same document, the undershoot exceeds -1.0 V in the SW waveform in Figure 15.
Is this "Figure 15" a mistake?

Q2)Is it no problem?
(Realy observed -1.0 V in the SW waveform at my target bord)

Q3)
Does this terminal have voltage specifications by AC characteristics?
(ex: short time overshoot and undershoot)

Remarks:
The same level of voltage is observed on the substrate being evaluated by our company, so we would like to judge whether there is a problem or not.

(Realy observed -1.0 V in the SW waveform)

If you have any information please let me know.

Best Regards

Shing