From the datasheet it says the charger is good for 1 to 4 cell designs
I have followed the design guidelines from the data sheet using a diode OR to power the device either from the input supply or from the battery.
However with a single cell Li-Ion battery with nominal voltage of 3.65, minus the voltage drop of the diode we will be well below the minimum VCC requirement of 4.5 from the data sheet when the system is running from the battery.
So do I need to include a boost converter on the battery before powering the charger or can the charger run at less than 4.5, if it can what is the lower limit of VCC for correct operation.