Can I change the setting of UVLO to 4.5V when startup in pinstrap mode?
Best Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can I change the setting of UVLO to 4.5V when startup in pinstrap mode?
Best Regards.
Hi Louis,
VIN_UVLO can not be changed via pin strap mode, however, you can change it on the fly thru PMBUS, here is the simple procedure.
1. While V5 reach UVLO, send PMBus command to TPS53647 to change VIN_UVLO.
2. Then make EN high.
Note1. You can issue "Store Config to NVM", then you will no need to change VIN_UVLO for every power up, or, you can change VIN_UVLO every power up without "Store Config to NVM"
Note2. VIN_UVLO can be changed on the fly regardless EN is high or low, it will take effect right away.
Thanks
Chasel
Hi Chasel
Thanks for your support.
Let me know the "Store Config to NVM".
If I do "Store Config to NVM", is it avalible to set of UVLO to 4.5V when startup in pinstrap mode?
Best regards.
Hi Louis,
Yes, if you store config to NVM, and after next power cycle, UVLO will be 4.5V unless you change the settings again.
Thanks
Chasel
Hi Louis,
Please check datasheet section 7.6.2.3.5.
SendByte to 11h.
Thanks
Chasel