I have a problem with TPS65131. It can not regulate under load.
Designed output voltage: +5V -5V
Symptoms:
1) Input voltage: 3.3V No load
-5v output: fluctuating between -2v and -12v (If I add large electrolytic cap to C28, -5v stable with no load, but with 50mA load it goes down to 0v)
+5v output: 5v stable
------------------------------------------------------------------------------------------
2) Input voltage: 3.3V 270mA load on both outputs
-5v output: 0v
+5v output: fluctuating between 3.6v and 3.85v
------------------------------------------------------------------------------------------
3) Input voltage: 5v No load
-5v output: -5v stable
+5v output: +5v stable
------------------------------------------------------------------------------------------
4) Input voltage: 5v 270mA load on both outputs
-5v output: 0v
+5v output: 4.7v (sometimes it goes down to 3v)
------------------------------------------------------------------------------------------
Schematic: https://i.hizliresim.com/p5NYb0.png
Board layout: https://i.hizliresim.com/kM8Y9W.png
Coil: vls3015cx-4r7m
Any help would be appreciated