Hi,
We are having one circuit with TPS65910A3A1RSL. Actually the circuit is made as required for push button press to low for power on function.
But it is not working like that. Device is powering on when supply is inserted to it without pressing push button. configuration is done as boot1 to Vrtc (1) and boot0 to ground (0) as this IC is being used with AM335X processor. Can anybody tell me what can be the problem here. And what is the role of VMBHI_IT_MSK bit of INT_MSK_REG register in this feature.
Thanks.