Other Parts Discussed in Thread: TPS63001
Hi, I designed a board with a TPS63031 regulator following both the recommended application circuit and the recommended layout (with one small change that I'll describe).
I produced about 40 boards at a processional assembly house. In about 10, the regulator fails to work. There is no voltage at the output (only a few mV). The rest work fine.
I need to understand and correct the reason for the failure before I produce more boards.
I disconnected the regulator from the rest of the circuit to eliminate any influence and it still fails.
The inductor is one of the recommended ones, Murata LQH3NPN1R5MJRL. The input and output capacitors are 10uF 16V ceramic caps, one at the input and two in parallel at the output. I tried to check the soldering of the inductor in one failed board but it seemed fine and resoldering did not fix the board.
What might have gone wrong in these boards and how can I diagnose and fix this?
Thanks, Sivan Toledo