This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79606A-Q1: OTUT DAC measurement process issue

Part Number: BQ79606A-Q1

Hi team,

In the datasheet of BQ79606 section 8.3.6.2, it says " TSREF must be enabled (CONTROL2[TSREF_EN]=1) for at least 2ms (for the recommended capacitor value, larger capacitors may lead to longer startup time) before enabling the OT/UT function".

But in the 8.3.6.4.1 section, step 5 enables UT/OT function before enabling the TSREF. Why is that?

Besides, I have another problem about the functional block diagram. As I can understand, the TSHUT PTAT should be the same physical input as the TWARN PTAT into the AUX ADC, because in the Table 5. AUX ADC I can only find the formula to calculate the TWARN_PTAT. Am I right?

Thank you for your reply!