Dear all,
I would like to ask a question.
I am looking for a reference design with a Cockcroft–Walton circuit.
I am trying to generate voltage from our customers under the following conditions
Input voltage: DC24V (DC20-30V)
Output voltage: DC6.6kV and -4.0kV
Output current: total 1 ~ 1.2mA
I believe that using the Cockcroft–Walton circuit can meet this requirement.
Therefore, we are looking for a reference design that satisfies this condition.
Is there a reference design with Cockcroft–Walton circuit under the above conditions?
Best Regards,
Y.Ottey