I am using the TPS544C25 to regulate a 3.3V output. The chip works fine and can regulate and load step, the only issue is that during startup, there is a small peak as the voltage rises from 0V to 3.3V. Whether it starts from no load or full load the issue still persists. I have attached a picture for reference. The yellow/orange line is the output voltage and the blue line is the voltage on the comp pin of the chip. I do not understand why the comp pin is going to 0 when the peaking occurs. I looked at the datasheet and the peaking seems to occur when the reference voltage hits the bottom of the ramp signal.
The converter operates from 12V to 3.3V.
If I start the converter up with some output voltage still on the capacitors, the startup rise is monotonic and everything works well.
Any help is appreciated thanks.