This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPS25944A: TPS25944A Pspice model work as TPS25942A:

Prodigy 225 points

Replies: 6

Views: 70

Part Number: TPS25944A

Hello,

I'm trying to simulate the following circuit and I'm expecting to see the current reach 1.2A for 4 ms then the the part should act as circuit breaker. 

As you can see from the simulation output the output current is limited to ILIM as specified in the TPS25942:

Datasheet reports:

The TPS25944 allows the overload current to flow through the device until I(LOAD) < I(FASTRIP). It starts the timer when I(LIM) < I(LOAD) < I(FASTRIP), and once the timer exceeds tCB(dly), the internal FET is turned off and FLT is asserted.

Could you tell me where is the mistake?

Thank you

  • Hi Alberto,

    Thanks for reaching out.

    Can you share me simulation file to check at my end.

    Best regards,

    Rakesh

    --------------------------------------------------------------------------------------------------------

    To find the latest information on Power Switches, Visit www.ti.com/powerswitch 

  • In reply to Alberto Burani:

    Hi Alberto,

    If the overload is during startup, even TPS25944 also limits the output current to Ilim for 4ms interval before shutting off.

    Best regards, Rakesh

    --------------------------------------------------------------------------------------------------------

    To find the latest information on Power Switches, Visit www.ti.com/powerswitch 

  • In reply to Rakesh:

    Thank for the answer, but can you tell me when the startup sequence ends and the device beging to work as tps25944? I did not find this information on the datasheet.

    Thank you

  • In reply to Alberto Burani:

    Hi Alberto,

    Startup sequence ends when the output voltage reaches close to Vin i.e., when the difference between Vout and Vin is just IR drop across the device.

    BR,

    Rakesh

    --------------------------------------------------------------------------------------------------------

    To find the latest information on Power Switches, Visit www.ti.com/powerswitch 

  • In reply to Rakesh:

    Ok, clear thanks for your support

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.