Other Parts Discussed in Thread: CC1310, TPS610981EVM-674
Hello,
We have a custom design that uses a TPS610986DSE powering a CC1310. At power-up, we have seen reset issues with the CC1310 depending on the voltage level applied to the TPS610986. We just received the TPS EVM and are verifying that the behavior we see is consistent when using our board or the EVM. If we remove the TPS device the CC1310 has no issue. When using the TPS, we see a fair amount of noise (150mV to 200mV) when the TPS device is in circuit and between the pass through and boost mode thresholds. If the supplied power input is under 3.1V and the device is in a continuous boost mode the CC1310 has no issue. We have also played with the overall tps current load. If we load the circuit with approx. 15mA the device functions as expected. Thus we are beginning to believe that perhaps we are managing to get the TPS in a unstable state.