Hi,
BQ35100 is designed to gauge non-rechargeable primary battery, Li-SOCI2 battery is used in my project, after reading datasheet of BQ35100, questions below need your help.
1, What's the temperature stability requirements of sense resistor between SRP & SRN during the overall operating temperature range?
2, In EOS mode, impedance tracking of primary battery is used to predict end-of-service status, so is it still needed to enable BQ35100 when major load pulse current is coming? If it is, the I2C port of BQ35100 should be connected to system controller which knows when major pulse load current come, and BQ35100 can not be configured to operate with a fixed period (24hours) no matter what load current.
3, BQ35100 has internal temperature sensor, is it used in EOS mode default?
Thanks.
Regards,
Ma Dawei