I AM USING DRIVER IN BUCK MODE WITH INPUT VOLTAGE 24V. IN OUTPUT I AM USING LED ARRAY (3 ROWS WITH EACH ROW HAVING 5 LEDS). AS SOON AS I SWITCHED ON POWER SUPPLY, LED ARRAY ALSO GET 6V WHICH CAUSES IT TO BE IN ON STATE (THOUGH VERY SMALL BRIGHTNESS). AND I HAVE NOT GIVEN ANY SIGNAL TO ENABLE PIN OF THE DRIVER. I AM USING BUCK CIRCUIT GIVEN IN DATA SHEET AS EXAMPLE.ITS MY REQUIREMENT THAT LED ARRAY MUST STAY OFF UNTIL UNLESS ENABLE SIGNAL IS PROVIDE.
ALSO IN BUCK CIRCUIT EXAMPLE L1 IS USED TWICE. IS IT REQUIRED OR IT’S A PRINTING MISTAKE.
KINDLY HELP ME