Other Parts Discussed in Thread: TPS61099
Hi,
I create a DC/DC power design in webench Power Design with this spec:
- VIN = 1.5V...2.8V;
- Vout = 3.3V;
- Imáx = 0.5A when transmit data during 10s;
- Inom < 50uA in sleep mode (most of time).
My board is powered with 2xCR2477(1000mAh each) battery.
The most efficiency design was with TPS61022RWUR but for my application I think the Quiescent Current is to high (around 27uA).
Can you suggest another IC with lower Quiescent Current?
Thank you,
Hélio Pereira