My battery is 7P6S, 12600mAh, and the sampling resistance is 1 mOhm. The BQ40Z80 only supports a maximum current of 32767mA. I need an instantaneous discharge current of 100-150A. Let's say I scale 5x. Is the following process right?
1) Use the standard 2A current to correct the current value.
2) The design capacity is set to 2520mAh.