So I have an issue when calibrating, I measure the voltage and fill in the box for 12000mV and calibrate the battery icon sees 12000mV but the percentage stays at 0%.
I have followed the steps in the video and on the evm datasheet exactly and i can't see why this is occurring.
I set the voltsel pin to 1, clicked reset, then calibrated the voltage followed by temp, cc offset & board offset, and then current with a 2A load connected.
Where have i gone wrong is there another bit that requires setting?
Is there a procedure to do a hard reset to factory settings so i can start again?
Kind regards,
Paddy