Other Parts Discussed in Thread: BQ24650
So, as I feared, I spent a lot of time and money on a new prototype design of the SLA-modified EVM circuit as you publish in SLVA437A (Using the bq24650 to Charge a Sealed, Lead-Acid Battery). Since you do not offer this modified design in an EVM, I had to "roll my own".
The design basically works (charger charges the battery), but there is something going on that has me stumped. When the charger is in Constant Current mode, the battery voltage begins to rise as expected. BUT IT NEVER REACHES THE 14.85V BULK CHARGE VOLTAGE. When the voltage does peak (~14.6) THE CHARGE CURRENT BEGINS TO DECLINE. The BQ24650 never switches out of CC mode, but the current begins to decline.
Can someone offer some perspective into what the heck is going on? Why would be current decline while still in CC mode? Why would the battery voltage never reach the 14.85 target?