This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

Mass of TPS7H4001-SP

Prodigy 60 points

Replies: 6

Views: 155

Could you please provide the mass of TPS7H4001-SP (18A POL).

  • I'll check to see if this information is available already.  If not, I'll put in the request to measure.  Will advise soon.

    Thanks

    Christian

  • In reply to Christian Yots:

    The mass for TPS7H4001-SP is 2485.69 grams.

    Thanks

    Christian

  • In reply to Christian Yots:

    I hope there is an error and that its mass is not 2.5kg ?

  • In reply to Dave Geerardyn:

    Sorry about that, left off the milli.  It is 2485.69mg.

    Thanks for correcting me.

    Christian

  • In reply to Christian Yots:

    Hi Christian,

    can you please confirm about the mass of TPS7H4001-SP

    because it is around 2.48Kg, which is higher mass

  • In reply to Supriya G R:

    mass is 2485.69mg or 2.486grams

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.