This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPS50601A-SP: PSRR for TPS50601A-SP

Expert 5445 points

Replies: 2

Views: 27

Part Number: TPS50601A-SP

Do we have any PSRR performance data (vs freq) for the TPS50601A-SP?

Does the spice model accurately predict PSRR?

Conditions:

3.3V -> 1.8V, 3A load, 100kHz, 10uH inductor, 1100uF output cap ( ~ 2mohm ESR effective), compensation = 1.74K & 220nF in parallel with 750pF

  • I am unable to find any PSRR data taken in Galileo. I will check with Daniel to see if he any measured data.

    Thanks,

    Christian

  • In reply to Christian Yots:

    We do not have any such measured data.

    -Thanks

    Christian

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.