This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL431: .

Part Number: TL431
Other Parts Discussed in Thread: UCC28740

I'm trying to design a power supply with the following calculations:

INPUT: 85VAC - 265VAC

OUTPUT: 80 volt, 0.6A

Topology: flyback with opto-coupler feedback

Voltage reference: TL431

controller IC: ucc28740

Transformer (designed using ucc28740 design calculator): PQ26/25 core, Nps = 1.172, Npa = 11.4, Lp = 172.6uH

The datasheet of TL431 states the maximum Vka = 37V, so I assume its not suitable for my use, but I found a flyback power supply design that uses the same TL431 for an output of 110 volts. I'm new to this kind of things hence require help...

thank you!