Other Parts Discussed in Thread: BQSTUDIO, , BQ34Z100-G1, GPCCHEM, BQ34Z100EVM, EV2400, BQ34Z100
Hi everyone,
I am evaluating the capabilities of the BQ34Z110 with the EVM and the Bqstudio. In Bqstudio I am able to change the battery chemistry, I apply reset and I can see the new CHEM ID has been written in the flash memory, however the battery capacity has not changed. I am using a Li ion 3.7V 2600mAh (https://www.sparkfun.com/products/12895). After changing the CHEM ID the registers windows still shows the Full Charge Capacity at 973mAh, even if I choose the model ICR18650-2600mA (CHEM_ID=0x1996) from the possible chemistries that Bq studio offers.
If the full charge capacity has not chaged, is the BQ34Z110 calculating the SOC properly?
What am I missing?
Best regards