Hi Team,
The maximum input voltage in the product page of LM317 in SOT-223 package shows that it is Vin (Max) = 40V. Upon checking the datasheet, there is no exact value of Vin. The Vin (Max) of 40V contradicts with the input-to-output differential voltage of VI - VO = 40V.
It also contradicts with the minimum output voltage of 1.25V if the input-to-output differential voltage is 40V because the total would be 41.25V.
What is the maximum input voltage of LM317DCY (SOT-223)?
Regards,
Danilo