Other Parts Discussed in Thread: LM25118
Based on TI's reference circuit, we designed it as follows.
VIN : 10V ~ 30V
VOUT : 12V
IOUT : 6A
However, for a 10V input, oscillation occurs at 2.5A load.
Best Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Based on TI's reference circuit, we designed it as follows.
VIN : 10V ~ 30V
VOUT : 12V
IOUT : 6A
However, for a 10V input, oscillation occurs at 2.5A load.
Best Regards
Hi Louis,
Thank you for reaching out with your question and for using the LM25118.
Can you please post a waveform capture of the output voltage? Also do you see this issue only when the ambient temperature is high?
Thanks,
Garrett
Hi Garrett
VIN : 10V ~ 30V
VOUT : 12V
IOUT : 6A
Ambient Temp : 70
Is the attached Webench design capable of 6A at 12V output from 10V input?
Please reply quickly.
Best Regards.