HI TI Team,
Duty cycle for TPS562201 has been 75% given in the datasheet.
Can we use the same part for 3.3V output with Minimum Input Voltage is 4.7V?
Please suggest the feedback.
Thanks
Saumil
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI TI Team,
Duty cycle for TPS562201 has been 75% given in the datasheet.
Can we use the same part for 3.3V output with Minimum Input Voltage is 4.7V?
Please suggest the feedback.
Thanks
Saumil
Hi Saumil,
Yes, TPS562201 can support this case. For your EE, do you have strict load transient requirement? what's your EE?
BRs,
Edwin.
Hi Edwin,
Ok, so basically we are using 5V,2A Adapter as input for our board and load current will not be more than 1.7A and we are using 2A adapter for the same.
Normally Adapters are in the range of +/-5% so considering that we just wanted to confirm that if for anytime output voltage of the adapter falls to 4.75V then also still we will be able to generate 3.3V from the switcher.
The same 3.3V Switcher output current requirement also not more than 1.5A.
Please let me know if you see any Risk in this.
Thanks
Saumil