I have a PoE PSE designed using TPS23861. The IC is not showing any activity -- no gate drive voltage to external FETs or drain voltages at MOSFET and will not respond via i2c (using broadcast address 30h, no ACK when sent commands).. Verified 3V3 on pins 1,2,24; verified GND on pins 7, 22, 11, & 18; verified 48V @ pin 28. Power is sequenced by external CPU -- 48V is turned on first, 500ms wait followed by 3V3. Not sure what else to check.