Other Parts Discussed in Thread: BQ35100, BQSTUDIO, , EV2400
my original application behaviour is like:
our device working is like it wake up 5 times a day, wake up period is nearly 60 sec and during this time take measurement from sensor and send data on zigbee and go to sleep,active mode current is nearly 80 mA and sleep mode is 1.6 mA. we are using two new Li-socl2 non rechargeable battery in parallel configuration(reason is that continuous current of one cell is 50ma so we use 2 cell in parallel to counter this situation).cell name is LS 14500 shaft battery.we need notification for battery change so for that we planning to use EOS mode of BQ35100.
Things i have:
BQ35100EVM-795 , BQstudio,EV2400 , battery pack of 2 primary shaft battery(LS14500) in parallel configuration.
Planning is first i test behaviour using BQ35100EVM-795 and than integrate it in original product.
Activity done till now is summarised here:
-install latest version of bqstudio and driver for ev2400.
-cross check all jumper as mentioned in doccument(on J2 jumper is on 1-s side and J3 on 2s).
-use load of 49ohm between BAT+ and -PACK to draw 70 mA current.
-done voltage,temperature and current calibration.
-change mode to EOS and other setting as per my understanding in data memory.
now to understand behaviour of measuredZ and scaled R i follow procedure(send start gauge->apply load for some second->remove load->send stop gauge command->wait for data to be updated->wait for 60 sec or more before repeat cycle)
i tested this with 2 type of battery for at least 3 above cycle,and log both measuredZ and scaled R in log
1- fully new battery(here i send new battery command also)
2-partially used battery
i find that after first cycle in both case both resister value is same i think it should be different. here is log file and other files(srec and data memory)
0100_1_02-bq35100_with_cal_EOS_mode.srec.txt
bq35100_data_memory_with_cal_EOS.gg.csv.csv
So what is standard procedure to test and validate my requirement?
what should be standard way to test it?
i also don't get why in both case values are same is i am doing it wrong?