Team,
I have some questions below:
1. To enter power state via command is to all devices on the stack but can it be done in any stack position?
2. Can host address parallel devices? I don't think so but just want to confirm.
Regards,
Allan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Allen,
A wakeup can be issued from any IC in the stack. Setting the DEV_CTRL[STACK_WAKE] bit will send the wake tone from the COMMH interface to all higher stacked ICs.
In regard to your second question about addressing parallel devices, can you please provide a diagram of what you are calling 'parallel devices'? The daisy-chain communications is connected to look like a series of ICs, but the physical connection to the cells can be in parallel if desired, though this is not common. The host can send a group broadcast or broadcast message which will address all ICs in a stack.
Is the customer designing a stack with multiple parallel strings of cells, instead of a series of parallel cells?