[?] 3 in one Voltage/Current/Temperature sensor max ~20V DC
is there such sensor exist? i see one in linear technology but only up to 5.5V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Devices in this battery management product line would be for monitoring individual cells in a 20 V battery along with current and temperature at levels common for lithium-ion battery. An example protector without communication would be the bq77905, there are a couple versions available now, new options need a supportable business case. For an I2C device the bq76920 is an option, but again with a battery focus. For other options you might try the TI cross reference search, or check for sensor products at www.ti.com/sensors . Parts such as the TMP512 or LM5056A would seem to support 20V.