Other Parts Discussed in Thread: BQ78350
Hi. I am being tested with BQ 76930EVM.
I intend to apply BQ76930 with 7S1P batteries to my system. (BQ76930 only, not BQ78350)
I have few questions.
1. Power Supply is connected Pack+ ,- for charging.
Charging is normal when "CHG" and "DSG" are ON, but not charging when only "CHG" is ON(DSG is off).
Is this normal operation?
2. If the PACK +,- of BQ76930 is connected to load, connect charge source to the PACK+,- to charge, will charge and discharge operate at the same time?
3. If the load has a discharge current of 1A and a 2A DC Adapter is connected at PACK+-, what is the charge / discharge operation and current?
Please let me know.
Thanks.