Beginner looking for some guidance on chip selection.
I have a 4S LiFePO4 battery that I wish to read the voltages across the entire battery as well as each cell. I do not require any additional features related to charging, balancing, temperature, etc. Just the voltages, so that I can read them into a microcontroller for output onto a display.
I did some research and found various solutions ranging from voltage dividers to opto-isolators, but none seemed to be ideal - they all either lacked in accuracy and/or safety. I then stumbled across the BQ76920 chip - but I am wondering if this chip is a bit of overkill for the application. Is this the right chip? Is there another chip/process that would be "better"? I am hoping for an accuracy of within 0.05V
Thank you all in advance!