Hi,
I want to know a few things about the bq76940 current measurement.
1) Do I need to set some bit to activate the full scale range? Because in the datasheet it says that the CC input voltage range is +-200mV and the full scale range is +-270mV.
Calculating the LSB we get (540mV)/(2^16) = 8.23 uV. Which is pretty close to the value given in the datasheet, 8.44 uV. So I assume that the full scale range is already activated. Is there any problem in working with this range?
2) Is there any way to enhance the current measurement precision of the bq76940? What is the usual guidance for it? Our system is a 48V/50Ah with current peaks of 150A
We thought about a PGA connected to its inputs (SRN/SRP) but we don't know if it's possible and how we control it.
Thank you,