I'm only seeing 1-2V on the CHG pin even though I have set the CHG_ON bit to 1 (I know the bit was written successfully because the CHG pin voltage is 0 before enabling CHG_ON). I am seeing ~12V at the DSG pin and there are no SYS_STAT bits being set other than CC_READY. I am using the exact schematic shown in section 7.3.1.3.1 of the datasheet. What could be the issue here?