HI,
When i send cmd 0x10 to EMB1428 then the CPU receive 0xA1 from EMB1428.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When i send cmd 0x10 to EMB1428 then the CPU receive 0xA1 from EMB1428.
Hi user, Cliff,
Error code 1010 means that done went high, and the error code from the emb1499 was not 000. It means that the emb1499 sent an error code of 010 to the emb1428. Error code 010 means that you hit the secondary side overcurrent limit of the DC-DC converter. You may need to reduce balancing current, change the sense resistor, etc to fix this. You may also want to ensure that you are giving the converter enough time to ramp down between balancing cycles.